The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

FB#.ENCLINES

Description

Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and will be ignored for any other encoders and linear motors.

Examples

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Lines/Rev

Range

0 to 4,294,967,288

Default Value

1024

Data Type

Integer
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
EtherCAT COE and CANopen FB1.ENCLINES 0x3500 0x2 UDINT - - RW False
FB2.ENCLINES 0x3501 0x2 UDINT - - RW False
FB3.ENCLINES 0x3502 0x2 UDINT - - RW False
FB4.ENCLINES 0x3503 0x2 UDINT - - RW False
FB5.ENCLINES 0x3504 0x2 UDINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen