The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

FB#.RESKTR

Description

This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.

The value can be obtained from the resolver data sheet.

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.001 to 50.000

Default Value

0.5

Data Type

Float

See Also

N/A
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
EtherCAT COE and CANopen FB1.RESKTR 0x3500 0x4 UDINT - - RW False
FB2.RESKTR 0x3501 0x4 UDINT - - RW False
FB3.RESKTR 0x3502 0x4 UDINT - - RW False
FB4.RESKTR 0x3503 0x4 UDINT - - RW False
FB5.RESKTR 0x3504 0x4 UDINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen