The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

FB#.RESREFPHASE

Description

This parameter sets the electrical degrees of phase lag in the resolver.

See the motor resolver datasheet for the value for this parameter.

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

electrical degrees

Range

-180 to 180°

Default Value

-2°

Data Type

Float

See Also

N/A
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
EtherCAT COE and CANopen FB1.RESREFPHASE 0x3500 0x5 UDINT - - RW False
FB2.RESREFPHASE 0x3501 0x5 UDINT - - RW False
FB3.RESREFPHASE 0x3502 0x5 UDINT - - RW False
FB4.RESREFPHASE 0x3503 0x5 UDINT - - RW False
FB5.RESREFPHASE 0x3504 0x5 UDINT - - RW False

Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen