The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

IP.GATEWAY

Description

This parameter is used to set the Gateway IP of the drive when IP.MODE is set to 1 for static IP. It determines the IP addresses the drive can communicate with outside of its current subnet.

Examples

Usage

IP.GATEWAY is only used when IP.MODE = 1. If communication with devices outside of the drive's subnet is desired then the Gateway IP should be set based on the IP address of devices outside of the subnet. The IP.RESET command can then be used to apply the specified IP settings.

Code

Set drive to be able to communicate with devices on 192.168.1.x subnet.

--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.GATEWAY 192.168.1.1
--> IP.RESET

Context

For more information on IP configuration, see Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read/Write
Units N/A
Range 0.0.0.0 to 255.255.255.255
Default Value 0.0.0.0
Data Type String
See Also IP.MODE, IP.ADDRESS, IP.SUBNET, IP.RESET

Stored in Non Volatile Memory

Yes

Variants Supported

All variants supported.


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen