Showing help for All Fieldbus and Functional Safety All
Select your Fieldbus
The model number will indicate what kind of fieldbus you have. Find the label on the side of the device, where "Model No:" is indicated. Modbus is included with all models.

All Fieldbuses

*E / *C

*P
Select your Functional Safety Version
The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

*1 (Functional Safety Option 1)

*2 (Functional Safety Option 2)

*3 (Functional Safety Option 3)
REGEN.REXT
Description
REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Ω |
Range |
0 to 330 Ω |
Default Value |
330 Ω |
Data Type |
Integer |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT COE and CANopen | REGEN.REXT | 0x3007 | 0x6 | UINT | - | - | RW | False |
Copyright © 2020 Kollmorgen
|
![]() |