The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

VBUS.ACNOMINAL

Description

This command configures the operating voltage for a level other than the default of the drive.


  • The drive can be de-rated but do not operate it higher than the original voltage.

When changed, VBUS.ACNOMINAL modifies the inrush voltage settings and the regen voltage configurations. It is important that VBUS.ACNOMINAL be set as accurately as possible to minimize voltage faults.

Examples

Code

If an HV drive (480V) was needed for bench testing at 120V, do the following:

VBUS.ACNOMINAL 120

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

VAC

Range

0 to Drive rated voltage

Default Value

Drive rated voltage

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

VBUS.DCNOMINAL

VBUS.DCOPERATION


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen