The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

Adding an Online Ethernet Device

To add an online Ethernet device to the project, perform the following.

  1. Select the device you want to add from the discovered devices.
  2. If the device you want to add does not appear, attempt manually specifying the IP address.
  3. Validate by pressing OK.


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen