The model number will indicate what kind of function safety you have. Find the label on the side of the device, where "Model No:" is indicated.

Apply
Clear Filters

Device Management

Device Representation

A device in WorkBench is represented by a node in the navigation top tree. A device node may be in one of several states:

  • Disconnected
  • Connected to a physical device through your network
  • Connected to a simulated device (sometimes called an "offline" device)

Device Identification

A physical device is identified by its serial number, which should be unique amongst all of them.


  • When connecting to a physical device, WorkBench will verify that you are connecting to the correct device using the identification stored in the project. WorkBench will warn you if the serial numbers are different, and ask if you want to continue.

Device Connection Information

Once you connect to a physical device through the network, WorkBench will store the connection information and reuse it in further connection attempts.


Stay Connected with Kollmorgen

Copyright © 2020 Kollmorgen