AXIS#.SAFE.VELOCITY
Description
Returns the safe velocity. This only returns a valid value when a safe encoder is attached to the considered axis.
Context
Related safety parameters:
- AXIS#.SAFE.ABSOLUTEPOSITION
- AXIS#.SAFE.ABSOLUTEPOSVALID
- AXIS#.SAFE.ACCELERATION
- AXIS#.SAFE.POSITION
- AXIS#.SAFEPARAM.ABSOLUTEPOSEN
- AXIS#.SAFEPARAM.ABSOLUTEPOSRANGE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
[-2^31+1, 2^31-1] |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |