AXIS#.SAFEPARAM.SSM_#.FUNCTIONACTIVATION

Description

Indicates the velocity upper limit of the Safe Speed Monitor (SSM) safety function. The parameter allows one of the following values:

Value Description

0

Never active

2

Always activated

This function can only be used when a safe encoder is configured in the safety parameters.

 

Context

For complete SSM information refer to SSM (Safe Speed Monitor).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 2

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSM_1.FUNCTIONACTIVATION

315fh

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSM_2.FUNCTIONACTIVATION

3160h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_1.FUNCTIONACTIVATION

325fh

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_2.FUNCTIONACTIVATION

3260h

01h

Unsigned8

-

-

Read/Write

No