SAFEPARAM.SIN.DISTINCTPULSE
Description
This setting indicates whether pulses on safe inputs must all be distinct from each other (i.e., offset from each other or different periods).
|
This does not disable the check for pulses on safe inputs. It only allows or disallows having the same pulse signal across safe inputs. |
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-01-02-000 |
|
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 (Disabled) or 1 (Enabled) |
Default Value |
0 (Disabled) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
SAFEPARAM.SIN.DISTINCTPULSE |
3101h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |