EXTENCODER.FREQ

Description

Gets the external encoder (EEO) velocity.

General Information

Type

R/O

Units

Hz

Range

-2^63 to +2^63 - 1

Default Value

0 Counts

Data Type

Float

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1078

No 32 bit No

M_01-05-11-000