EXTENCODER.POSMODULO

Description

Sets/gets the external encoder (EEO) modulo position.

General Information

Type

R/W

Units

1/(2^64)

Range

0 to +2^64 - 1

Default Value

0 Counts (off)

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1084

Yes 64 bit No

M_01-05-11-000