DRV.SWENABLE

Description

The following commands disable or enable the drive:

  • 0 (disables the drive)
  • 1 (enables the drive)

Before power can flow to the motor, the following must all be true:

  1. Drive is not faulted.
  2. DRV.SWENABLE* input (J4-6) is connected to I/O RTN.
  3. DRV.SWENABLE Parameter is set to 1.

General Information

Type

R/W Parameter

Units

none

Range

0 to 1

Default Value

0

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1056

No 8 bit No

M_01-05-11-000

Related Topics

DRV.ACTIVE