EGEAR.ERROR
Description
EGEAR.ERROR is never automatically set to zero. It accumulates position deviation each time acceleration limiting is activated. Typically, set EGEAR.ERROR to zero before doing something that activates acceleration limiting.
The slave axis’ acceleration or deceleration is limited to EGEAR.ACCLIMIT or EGEAR.DECLIMIT whenever:
- Gearing is turned on or turned off.
- Ratio is changed.
- EGEAR.PULSESIN or EGEAR.PULSESOUT is changed.
Example
EGEAR.ACCLIMIT = 10000 EGEAR.PULSESIN = 1 EGEAR.PULSESOUT = 1 EGEAR.ERROR = 0 EGEAR.TYPE = 0 EGEAR.ON = 1 While EGEAR.LOCK = 0 : wend MOVE.RELATIVEDIST = EGEAR.ERROR MOVE.GOREL 'catch up the position lost while acceleration was being limited
General Information
Type |
R/W |
Units |
Position counts |
Range |
-140,737,488,355,328 to 140,737,488,355,328 |
Default Value |
0 |
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1064 |
Yes | low 32 bit word | No |
M_01-05-11-000 |
Related Topics