VM.AUTOSTART
Description
VM.AUTOSTART specifies whether or not the program in the AKD BASIC starts executing automatically when DC power is applied.
- 0 = Program does not start automatically
- 1 = Program starts automatically
Set VM.AUTOSTART to 0 or 1 in the terminal in WorkBench and execute an NVSave.
General Information
Type |
R/W |
Units |
none |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1152 |
No | 32 bit | No |
M_01-05-11-000 |