VM.RESTART
Description
Causes program execution to start again from the beginning of the program. Restart is the only way to exit from an Error Handler routine. Any interrupts, WHEN statements or loops in progress will be aborted.
-
-
VM.RESTART does not clear the user program variables or change any program variables, any predefined variables or have any effect on motor motion by itself .
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1154 |
No | Command | No |
M_01-05-11-000 |
Related Topics
VM.START | VM.STOP