FBUS.SYNCWND
Description
This parameter sets symmetrically arranged window around the desired sync distance.
General Information
Type |
NV Parameter |
Units |
ns |
Range |
0 to 1,000,000 ns |
Default Value |
50,000 ns |
Data Type |
Integer, U2 |
See Also |
Appendix B: Fieldbus Manuals |
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Index/Subindex | Object Start Version |
---|---|
3496h/3 | M_01-00-00-000 |
Fieldbus | Address | Attributes | Signed? |
---|---|---|---|
PROFINET |
2181 | DWord | No |
Sercos® III | 4 Octets |
Instance | Data Size | Data Type |
---|---|---|
182 | 4 Byte | Integer |
Index/Subindex | Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|
362 |
No | 32 bit | No | M_01-03-00-000 |