MODBUS.ERRORS

Description

Lists up to 125 Modbus errors. Each entry contains the Modbus address and the error code of the failed Modbus request.

If more than 125 errors occur, the oldest error is dropped and the new error is stored at the end of this list. All Modbus errors are stored regardless of the state of the error mode (MODBUS.ERRORMODE).

Access Through Telnet

Telnet or the WorkBench terminal will display the entire list:

-->MODBUS.ERRORS
Error count: 2
[00384]   6 : Argument lower than minimum.
[00390] 109 : Invalid Register address.

Access Through Modbus

In Modbus the error list starts at register address 0x1102 (4354).

Modbus Address Description
4354 Error count
4355 Error 1 : Register Address
4356 Error 1 : Error Code
4357 Error 2 : Register Address
4358 Error 2 : Error Code
... ...
4603 Error 125 : Register Address
4604 Error 125 : Error Code

General Information

Type

R/O

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-08-03-001

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET No
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Related Topics

MODBUS.ERRORMODE | MODBUS.CLRERRORS