Download AKD PDMM Drive Firmware
Component | Title | Download Link |
---|---|---|
800MHz AKD PDMM Drive FW Firmware |
(AKD-M-MCEC-[firmware version]) |
|
1.2GHz AKD PDMM Drive FW |
(AKD-M-M1EC-[firmware version]) |
Update the AKD PDMM Drive Firmware with KAS-IDE
- In the toolbar, deactivate the Online Configuration Mode.
- Select the drives requiring the same firmware version to be updated.
The firmware download is limited to 16 drives at a time.
- Click the Upgrade Firmware button.
Warning dialogs may appear at this point.
These warnings include important information about preventing damage to the drives.
- Browse to the new AKD/AKD2G firmware file.
See the Release Notes for the latest supported firmware. - Click Open to start the updating procedure.
This procedure is not possible when applications are running and when the drive is in Online Configuration Mode.