FSoEParamsInit
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Transfers safety parameters from the safety master to safety slave devices to initialize the safety network.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
TRUE, FALSE |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge. the function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block initiates safety parameter transfer from the FSoE master at address FSoEMasterAddres to its safety slaves. |
INT |
-32768 to +32767 |
N/A |
No default |
The EtherCAT slave address of the FSoE master that is asked to initialize safety parameters. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
FALSE, TRUE |
N/A |
Indicates whether this function block has completed without error. |
Error |
BOOL |
FALSE, TRUE |
N/A |
Indicates whether this function block has completed with error. |
ErrorID |
DINT |
No range |
N/A |
The parameter initialization error result.
|
Remarks
This function block reads the safety parameters from the
- The function block:
- Checks the FSoE master's register for the safety parameter transfer on the rising edge of the Execute input.
- Gets the EtherCAT address of the safety slave that receives the safety parameter if the FSoE master has any safety parameters to transfer.
- Once the address is read and validated from the FSoE master, the function block reads the actual parameter from the FSoE master and writes the parameter to the safe slave.
- The Done output is set to 1 when all parameters to all of the intended Safety slaves are written.
- The Error output is set to 1 and the appropriate ErrorID is set in the ErrorID output if any error occurred during this process.
- FSoE masters supported by this function block: BBH SCU-1-EC
Figure 1: FSoEParamsInit
EtherCAT Error Codes
Value Dec (hex) |
Error Code |
Description |
---|---|---|
0 |
ECERR_OK |
The SDO call succeeded. |
1000 (0x3E8) |
ECERR_DEVICE_ACTION_IS_INVALID |
The requested Device Action is invalid. |
1003 (0x3EB) |
ECERR_DEVICE_ACTION_MINIMUM_ONE_NODE_REQD |
A minimum of one device must be present in the EtherCAT network. |
1004 (0x3EC) |
ECERR_DEVICE_ACTION_MINIMUM_ONE_DC_NODE_REQD |
A minimum of one Distributed clock Clock signal. capable device must be present in the EtherCAT network. |
107 = 0x6B |
The size of the connections is too small.
|
|
1792 (0x700) |
ECERR_DEVICE_ERROR |
EtherCAT device is not accessible. |
1794 (0x702) |
ECERR_DEVICE_INVALIDCMD |
Invalid mailbox command. |
1795 (0x703) |
ECERR_DEVICE_INVALIDINDEX |
An invalid value for the Index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. input was specified. |
1796 (0x704) |
ECERR_DEVICE_INVALIDACCESS |
Reading of the variable is not permitted. |
1797 (0x705) |
ECERR_DEVICE_INVALIDSIZE |
An invalid size for the parameter was specified. |
1798 (0x706) |
ECERR_DEVICE_INVALIDDATA |
Invalid parameter value(s) in SDO index and/or sub-index. |
1799 (0x707) |
ECERR_DEVICE_NOTREADY |
Device is not in a ready state. The network is not in operational. |
1800 (0x708) |
ECERR_DEVICE_BUSY |
Device is not available to respond. |
1801 (0x709) |
ECERR_DEVICE_INVALIDCONTEXT |
Device responded with an illegal error code, indicating the command is not allowed under the present conditions. |
1802 (0x70A) |
ECERR_DEVICE_NOMEMORY |
EtherCAT mailbox is out of memory or device is out of disk space. |
1803 (0x70B) |
ECERR_DEVICE_INVALIDPARM |
EtherCAT mailbox request was not valid. |
1804 (0x70C) |
ECERR_DEVICE_NOTFOUND |
EtherCAT device not found. |
1805 (0x70D) |
ECERR_DEVICE_SYNTAX |
An unexpected error occurred. |
1810 (0x712) |
ECERR_DEVICE_INVALIDSTATE |
The EtherCAT device is in an invalid state. |
1817 (0x719) |
ECERR_DEVICE_TIMEOUT |
|
1826 (0x722) |
ECERR_DEVICE_INSERTMAILBOX |
Error while inserting the mailbox command into internal FIFO. |
1827 (0x723) |
ECERR_DEVICE_INVALIDOFFSET |
An invalid value for the SubIndex input was specified. |
1828 (0x724) |
ECERR_DEVICE_UNKNOWNMAILBOXCMD |
The master sent an unknown mailbox command to the slave. |
1829 (0x725) |
ECERR_DEVICE_ACCESSDENIED |
Device responded with an invalid access error code, indicating the command is not allowed. |
1832 (0x728) |
ECERR_DEVICE_INVALIDADDR |
The specified EtherCAT node address is invalid. |
1836 (0x72c) |
ECERR_DEVICE_NOT_A_FSOE_MASTER |
Device is not a FSoE master. |
1837 (0x072D) |
ECERR_DEVICE_DISCONNECTED |
The EtherCAT device is disconnected. |
1920 (0x780) |
ECERR_DEVICE_PARAM_ACCESS_ERROR |
Unknown error occurred while accessing parameter. |
1921 (0x781) |
ECERR_DEVICE_PARAM_NOT_FOUND |
Parameter was not found. |
1922 (0x782) |
ECERR_DEVICE_PARAM_NOT_INTEGER |
Parameter is a floating-point value. Integer value required. |
1923 (0x783) |
ECERR_DEVICE_VALUE_IS_NEGATIVE |
No negative values allowed. Value specified was negative. |
1924 (0x784) |
ECERR_DEVICE_VALUE_OUT_OF_RANGE |
Value is out of data-range. |
1925 (0x785) |
ECERR_DEVICE_VALUE_GREATER_THAN_MAX |
Value bigger than maximum. |
1926 (0x786) |
ECERR_DEVICE_VALUE_LOWER_THAN_MIN |
Value lower than minimum. |
2048 (0x800) |
ECERR_CLIENT_ERROR |
Error in Mailbox response to a previously sent mailbox command. |
2049 (0x801) |
ECERR_CLIENT_TIMEOUT |
The SDO command timed out. |
2050 (0x802) |
ECERR_CLIENT_ INVALIDPARM |
An invalid value was specified. |
2051 (0x803) |
ECERR_CLIENT_ INVALIDSIZE |
An invalid value for the size input was specified. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_FSoEParamsInit(True, EtherCAT.FSoE_Mst_1);
See Also