Axis Function Examples
MLAxisMoveVel(Speed)
- MLAxisMoveVel(Speed Speed is the absolute value of the velocity without direction.) starts to run the axis.
- MLAxisGenIsRdy returns TRUE when the Speed is reached.
MLAxisMoveVel(0.0)
- MLAxisMoveVel(0.0) reduces the speed down to 0 (zero).
- MLAxisGenIsRdy returns TRUE once the axis is ready.
Figure 1: Axis Functions Usage