MLAxisReadUUnits
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Gets the User units per revolution value of the axis.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OK |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
UserUnitsPerRev |
LREAL |
|
|
Returns the Axis User Units per revolution. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Axis1_User_Units := MLAxisReadUUnits(PipeNetwork.Axis1 ) ;