MLPrfReadOScale
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the Output Ratio value of a selected CAM Profile The position of a slave axis is mathematically linked to the position of a master axis. Example: A system where two rotating drums turn at a given ratio to each other. A more advanced case of electronic gearing is electronic camming. With electronic camming, a slave axis follows a profile that is a function of the master position. This profile need not be linear but it must be a mathematical function..
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
ProfileID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initialized CAM Profile. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Ratio |
LREAL |
|
|
Returns the Output Ratio value of a selected CAM Profile. |
Remarks
- Previous function name: MLPrfGetORatio
- Ratios can be changed on the fly to modify the CAM Profile while maintaining its basic shape.
- A change in output ratio is equivalent to stretching, and flipping if negative, the CAM Profile on the Y (or Output) Axis.
Figure 1: MLPrfReadOScale
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Save value of output ratio
CamRatio := MLPrfReadOScale( Profiles.Profile_A );
See Also