MLCompReset
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Clears the Transition Flag of a comparator Pipe Block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Comparator object. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE when function starts to execute. |
Remarks
- The Transition Flag of a comparator object turns TRUE if the input position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. to the comparator is greater or equal to the reference.
- The Comparator Transition Flag stays TRUE until it is reset New start of the microprocessor..
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Clear the Transition Flag of a Comparator object
MLCompReset( PipeNetwork.MyComp );
See Also