MLPmpStatus
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the status of the PMP block generator.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
EN |
BOOL |
FALSE, TRUE |
N/A |
No default |
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a PMP function block A function block groups an algorithm and a set of private data. It has inputs and outputs. in the Pipe Network. |
Outputs
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
PMP_Status := MLPmpStatus ( PipeNetwork.PmpMaster ) ;
Done :=TRUE;