MLPipeCreate
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Create a new pipe object.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Name |
STRING |
No range |
N/A |
No default |
Name for the newly created Pipe. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
ID |
DINT |
|
|
Assigned ID number of the created Pipe. |
Remarks
A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between.
-
-
Pipes are created in the Pipe Network using the graphical engine.
You do not have to add MLPipeCreate function blocks A function block groups an algorithm and a set of private data. It has inputs and outputs. to their programs The act of performing a sequence of instructions or commands..
The code with MLPipeCreate commands are automatically generated and called in a program with PipeNetwork(MLPN_CREATE_OBJECTS).
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create a new pipe
PipeAXIS1 := MLPipeCreate( 'PipeAXIS1' );
See Also
- MLPipeAct
- MLPipeAddBlock
- MLPipeDeact
- Pipe Network Functions for the PLC - MLPN_CREATE_OBJECTS