MLSmpConPNAxis
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Connects a sampler block to a specific Pipe Network axis variable.
Inputs
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Function block is operational. |
Remarks
Figure 1: MLSmpConPNAxis
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a sampler block named “SAMPLER” to a variable named ML_PIPE_POSITION from a Pipe Network Axis named PipeNetwork.AXIS1
MLSmpConPNAxis( PipeNetwork.SAMPLER , PipeNetwork.AXIS1, ML_PIPE_POSITION );