MLSyncStart
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Starts a synchronization Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. of a synchronizer Pipe Block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Pipe Network Block. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Function block A function block groups an algorithm and a set of private data. It has inputs and outputs. executed successfully. |
Remarks
Returns TRUE if the function succeeded.
Figure 1: MLSyncStart
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLSyncStart( PipeNetwork.SYN );