MLSyncStop
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - De-synchronizes a synchronizer Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. Pipe Block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
LREAL |
No range |
User units |
No default |
Motion Stop Position. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Function block A function block groups an algorithm and a set of private data. It has inputs and outputs. executed successfully. |
Remarks
Returns TRUE if the function succeeded.
Figure 1: MLSyncStop
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLSyncStop( PipeNetwork.SYN , 120 );