RAMP
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL |
|
|
|
Input signal. |
ASC |
REAL |
Maximum ascendance during time base. |
|||
DSC |
REAL |
Maximum descendant during time base. |
|||
TM |
TIME |
Time base. |
|||
RST |
BOOL |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OUT |
REAL |
|
|
Remarks
- Parameters are not updated constantly.
- They are taken into account only when the:
- The block is called the first time.
- Reset input (RST) is TRUE.
- In these two situations, the output is set to the value of IN input.
- They are taken into account only when the:
- ASC and DSC give the maximum ascendant and descendant growth during the TB time base.
Time Diagram
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
(* MyRamp is a declared instance of RAMP function block A function block groups an algorithm and a set of private data. It has inputs and outputs. *)
Op1: CAL MyRamp (IN, ASC, DSC, TM, RST)
FFLD MyBlinker.OUT
ST Structured text - A high-level language that is block structured and syntactically resembles Pascal. OUT
ST Language Example
(* MyRamp is a declared instance of RAMP function block *)
MyRamp (IN, ASC, DSC, TM, RST);
OUT := MyBlinker.OUT;