SigID
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
SIGNAL |
STRING |
|
|
|
Name of the signal resource. Must be a constant value. |
COL |
STRING |
|
|
|
Name of the column within the signal resource. Must be a constant value. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
ID |
DINT |
|
|
ID of the signal to be passed to other blocks. |
Remarks
- Some blocks have arguments that refer to a signal resource.
- For all these blocks, the signal argument is materialized by a numerical identifier.
FBD Language Example
FFLD Language Example
IL Language Example
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. 'MySignal'
SigID 'FirstColumn'
ST ID
ST Language Example
ID := SigID ('MySignal', 'FirstColumn');
See Also