SurfLin
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
X |
REAL |
|
|
|
X coordinate of the point to be interpolated. |
XAxis |
REAL[ ] |
|
|
|
X coordinates of the known points of the X axis. |
Y |
REAL |
|
|
|
Y coordinate of the point to be interpolated. |
YAxis |
REAL[ ] |
|
|
|
Y coordinates of the known points of the Y axis. |
ZVal |
REAL[ ] |
|
|
|
Z coordinate of the points defined by the axis. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
ERR |
DINT |
|
|
|
OK |
BOOL |
|
|
TRUE if successful. |
Z |
REAL |
|
|
Interpolated Z value corresponding to the X,Y input point. |
Remarks
This function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. performs linear surface interpolation in between a list of points defined in XAxis and YAxis single dimension arrays.
- The output Z value is an interpolation of the Z values of the four rounding points defined in the axis.
- Z values of defined points are passed in the ZVal matrix (two dimension array).
- ZVal dimensions must be understood as: ZVal [ iX , iY ]
- Values in X and Y axis must be sorted from the smallest to the biggest.
- There must be at least two points defined in each axis.
- ZVal must fit the dimension of XAxis and YAxis arrays.
- For instance:
- XAxis : ARRAY [0..2] of REAL;
- YAxis : ARRAY [0.3] of REAL;
- ZVal : ARRAY [0..2,0..3] of REAL;
- For instance:
- If the input point is outside the rectangle defined by XAxis and YAxis limits, the Z output is bound to the corresponding value and an error is reported.
If the function fails, the ERR output gives the cause of the error:
Error Code |
Meaning |
---|---|
0 |
OK |
1 |
Invalid dimension of input arrays. |
2 |
Invalid points for the X axis. |
3 |
Invalid points for the Y axis. |
4 |
X,Y point is out of the defined axis. |
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.