f_trig
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
CLK |
BOOL |
|
|
|
Boolean signal. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
TRUE when the input changes from TRUE to FALSE. |
Remarks
- It is recommended to use declared instances of R_TRIG or F_TRIG function A function calculates a result according to the current value of its inputs.
A function has no internal data and is not linked to declared instances. blocks.
- This is to avoid contingencies during an Online Change Applies to downloading PLC code changes while the applicaiton is running..
Truth Table
CLK |
CCLK (prev) |
Q |
---|---|---|
0 |
0 |
0 |
0 |
1 |
1 |
1 |
0 |
0 |
1 |
1 |
0 |
FBD Language Example
FFLD Language Example
- In the FFLD Language, ]P[ and ]N[ contacts can be used.
IL Language Example
(* MyTrigger is declared as an instance of F_TRIG function block *)
Op1: CAL MyTrigger (CLK)
LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. MyTrigger.Q
ST Q
ST Language Example
(* MyTrigger is declared as an instance of F_TRIG function block. *)
MyTrigger (CLK);
Q := MyTrigger.Q;
See Also