XOR / XORN
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN1 |
BOOL |
|
|
|
First Boolean input. |
IN2 |
BOOL |
|
|
|
Second Boolean input. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
Exclusive OR of all inputs. |
Remarks
- The block is called =1 in FBD Function block diagram - Describes a function between input variables and output variables. A function is described as a set of elementary blocks. and FFLD languages.
Truth Table
IN1 | IN2 | Q |
---|---|---|
0 |
0 |
0 |
0 |
1 |
1 |
1 |
0 |
1 |
1 |
1 |
0 |
FBD Language Example
FFLD Language Example
- The first input is the rung.
- The rung is the output.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly.
language, the XOR instruction performs an exclusive OR between the current
result and the operand.
- The current result must be Boolean.
- The XORN instruction performs an exclusive between the current result and the Boolean negation of the operand.
Op1: FFLD IN1
XOR IN2
ST Q (* Q is equal to: IN1 XOR IN2 *)
Op2: FFLD IN1
XORN IN2
ST Q (* Q is equal to: IN1 XOR (NOT IN2) *)
ST Language Example
Q := IN1 XOR IN2;
Q := IN1 XOR IN2 XOR IN3;
See Also