DTListTimeZones
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - List the time zones available on the controller.
This function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is specific for PCMM2G only.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
TRUE, FALSE |
N/A |
No default |
If TRUE, request to read the available time zones. |
TimeZones |
STRING[ ] |
No range |
N/A |
No default |
An array where the list of time zones available on the system are copied. This is effectively an output parameter, but because it is an array, it must be an input. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, the command completed successfully. |
Error |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, an error has occurred. |
ErrorID |
DINT |
No range |
N/A |
Indicates the error if Error output is TRUE. Error Codes
|
TZCount |
DINT |
No range |
N/A |
The number of time zones on the system. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// read the list of supported time zones
Inst_DTListTimeZones( bListDTZones, TimeZones );
if NOT Inst_DTListTimeZones.Error then
TZCount := Inst_DTListTimeZones.TZCount;
else
ErrorID := Inst_DTListTimeZones.ErrorID;
end_if;
if Inst_DTListTimeZones.Done then
bListDTZones := false;
end_if;
See Also