DTEvery
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Generate a pulse When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated. signal with long period Motor systems having a reciprocating or oscillating motor that operates synchronously with the periodicity of the source which supplies the electrical energy. The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input pipe block..
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Run |
BOOL |
TRUE, FALSE |
N/A |
No default |
When TRUE, the signal generation is enabled Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive.. |
Days |
DINT |
1 to 65536 |
Days |
No default |
Period : number of days. |
TM |
Time |
0 to 86,399,999 |
Milliseconds |
No default |
Rest of the period (if not a multiple of 24h). |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
TRUE, FALSE |
N/A |
Pulse signal. |
Remarks
- This function A function calculates a result according to the current value of its inputs.
A function has no internal data and is not linked to declared instances. block provides a pulse signal with a period of more than 24h.
- The period
is expressed as:
DAYS * 24h + TM
- The period
is expressed as:
- Example: Specifying DAYS=1 and TM=6h means a period of 30 hours.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MyDTEVERY is a declared instance of DTEVERY function block. *)
MyDTEVERY (RUN, DAYS, TM);
Q := MyDTEVERY.Q;
See Also