List of Date / Time / NTP ErrorID Codes
- 23 = Internal error.
See the controller log for details. - 15000 = Controller type does not support this function block A function block groups an algorithm and a set of private data. It has inputs and outputs..
- 16200 = Could not read NTP server configuration file.
- 16201 = Invalid time zone.
- 16202 = Cannot set date / time when NTP synchronization Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. is active.
- 16203 = Invalid date / time value specified.