bcd_to_bin
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
DINT |
|
|
|
Integer value in BCD. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
DINT |
|
|
Converts a Binary Coded Decimal (BCD) value to a binary value. Value converted to integer or 0 (zero) if IN is not a valid positive Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. BCD value. |
Remarks
- The input must:
- Be positive.
- Represent a valid BCD value.
Truth Table
IN |
Q |
---|---|
-2 |
0 (invalid) |
0 |
0 |
16 (16#10) |
10 |
15 (16#0F) |
0 (invalid) |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the input must be loaded in the current result before calling the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
BCD_TO_BIN
ST Q
ST Language Example
Q := BCD_TO_BIN (IN);
See Also