acos / acosL
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL / LREAL |
|
|
|
Real value. |
Outputs
Output |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Q |
REAL / LREAL |
|
|
|
Result: Arc-cosine of IN. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the first input must be loaded before the function call.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
ACOS
ST Q (* Q is: ACOS (IN) *)
ST Language Example
Q := ACOS (IN);
See Also