expt
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculates a power.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL |
|
|
|
Real value. |
EXP |
DINT |
|
|
|
Exponent. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
REAL |
|
|
Result: IN at the EXP power. |
Remarks
The exponent (second input of the function) must be the operand of the function.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the conversion is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the input must be loaded in the current result before calling the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
EXPT EXP
ST Q (* Q is: (IN ** EXP) *)
ST Language Example
Q := EXPT (IN, EXP);
See Also