CycleStop
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
BOOL |
FALSE, TRUE |
|
|
Condition. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
FALSE, TRUE |
|
TRUE if performed. |
Remarks
- This function turns the Virtual Machine The complete assembly of all connected parts or devices, of which at least one is movable. in Cycle Stepping mode.
- Restarting normal execution is performed using the debugger.
- The VM is set in Cycle Stepping mode only if the IN argument is TRUE.
- The current program The act of performing a sequence of instructions or commands. and any sub-programs called by the current program execute to the end of their cycle.
- Other programs are not executed.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also