EnableEvents
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
EN |
BOOL |
FALSE, TRUE |
|
|
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
ENO |
BOOL |
FALSE, TRUE |
|
Echo of EN input. |
Remarks
- Production is enabled when the application starts.
- The first production is operated after the first cycle.
- To disable events since the beginning, you must call EnableEvents (FALSE) in the very first cycle.
FBD Language Example
FFLD Language Example
- The input rung (EN) enables the event production.
- The output rung keeps the state of the input rung.
- Events are enables if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the first input must be loaded before the function call.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. EN
EnableEvents
ST ENO
ST Language Example
ENO := EnableEvents (EN);
See Also