and_mask
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
ANY |
|
|
|
First input. |
MSK |
ANY |
|
|
|
Second input. (AND mask) |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
ANY |
|
|
AND mask between IN and MSK inputs. |
Remarks
- Arguments can be signed or unsigned integers from 8- to 32-bits.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set.
Both are required for enabling the drive. the operation.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO is equal to EN.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the first parameter (IN) must be loaded in the current result before calling the function.
- The other input is the operands of the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
AND_MASK MSK
ST Q
ST Language Example
Q := AND_MASK (IN, MSK);
See Also