ascii
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
STRING |
|
|
|
Input string. |
POS |
DINT |
|
|
|
The first valid character position is 1. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
CODE |
DINT |
|
|
Either:
|
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set.
Both are required for enabling the drive. the operation.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the first parameter (IN) must be loaded in the current result before calling the function.
- The other input is the operand of the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
AND_MASK MSK
ST CODE
ST Language Example
CODE := ASCII (IN, POS);
See Also