left
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
STRING |
|
|
|
Character string. |
NBC |
DINT |
|
|
|
Number of characters to extract. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
STRING |
|
|
String containing the first NBC characters of IN. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the first input (the string) must be loaded in the current result before calling the function.
- The second argument is the operand of the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. IN
LEFT NBC
ST Q
ST Language Example
Q := LEFT (IN, NBC);
See Also