StringToArray / StringToArrayU
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
SRC |
STRING |
|
N/A |
No default |
Source STRING. |
DST |
SINT |
|
N/A |
No default |
Destination array of SINT small integers. USINT for StringToArrayU. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
DINT |
|
N/A |
Number of characters copied. |
Remarks
This function:
- Copies the characters of the SRC string to the first characters of the DST array.
- Checks the maximum size destination arrays and reduces the number of copied characters if necessary.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
- In the IL Instruction list - This is a low-level language and resembles assembly. Language, the input must be loaded in the current result before calling the function.
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. SRC
StringToArray DST
ST Structured text - A high-level language that is block structured and syntactically resembles Pascal. Q
ST Language Example
Q := StringToArray (SRC, DST);
See Also