TMU / TMUsec
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
BOOL |
FALSE, TRUE |
|
|
The time counts Internal count pulses, 1 pulse = 1/2^20turn. when this input is TRUE. |
RST |
BOOL |
FALSE, TRUE |
|
|
Timer is reset New start of the microprocessor. to 0 (zero) when this input is TRUE. |
PT |
TIME |
|
|
|
Programmed The act of performing a sequence of instructions or commands. time. (TMU) |
PTsec |
UDINT |
|
|
|
Programmed time. (TMUsec - seconds) |
Outputs
Input |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
FALSE, TRUE |
|
Timer elapsed output signal. |
ET |
TIME |
|
Elapsed time. (TMU) |
|
ETsec |
UDINT |
|
Elapsed time. (TMU - seconds) |
Remarks
TMUsec is identical to TMU except that the parameter is a number of seconds.
- The timer counts up when the IN input is TRUE.
- It stops when the programmed time is elapsed.
- The timer is reset when the RST input is TRUE.
- It is not reset when IN is false.
Time Diagram
Figure 1: Time Diagram
FBD Language Example
FFLD Language Example
IL Language Example
(* MyTimer is a declared instance of TMU function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MyTimer (IN, RST, PT)
FFLD MyTimer.Q
ST Q
FFLD MyTimer.ET
ST ET
ST Language Example
(* MyTimer is a declared instance of TMU function block *)
MyTimer (IN, RST, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;
See Also