TP / TPR
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
BOOL |
FALSE, TRUE |
|
|
Timer command. |
PT |
TIME |
|
|
|
Programmed The act of performing a sequence of instructions or commands. time. |
RST |
BOOL |
FALSE, TRUE |
|
|
Reset New start of the microprocessor. (TPR only). |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
FALSE, TRUE |
|
Timer elapsed output signal. |
ET |
TIME |
|
|
Elapsed time. |
Remarks
- TPR is same as TP but has an extra input for resetting the timer.
- The timer starts on a rising pulse of IN input.
- It stops when the elapsed time is equal to the programmed time.
- A falling pulse of IN input resets the timer to 0 (zero) but only if the programmed time is elapsed.
- All pulses of IN while the timer is running are ignored.
- The output signal is set to TRUE while the timer is running.
Time Diagram
Figure 1: Time Diagram
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung is the IN command.
- The output rung is Q the output signal.
IL Language Example
(* MyTimer is a declared instance of TP function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MyTimer (IN, PT)
FFLD MyTimer.Q
ST Q
FFLD MyTimer.ET
ST ET
ST Language Example
(* MyTimer is a declared instance of TP function block *)
MyTimer (IN, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;
See Also