Search IndexFile and TCP/IP Function Block ErrorIDs
This is the list of possible errors that could be returned at the ErrorID output of the File Tools Function Blocks and Search IndexTCP/IP Function Blocks.
File ErrorIDs
ErrorID |
Description |
---|---|
16000 |
Error opening file. |
16001 |
|
16002 |
File ID is invalid. |
16003 |
File ID has been closed. |
16004 |
Error in file stream. |
16005 |
End of file encountered. |
16006 |
Internal file FB error. |
16007 |
Unknown file error. |
16008 |
No such file or directory. |
16009 |
Bad file descriptor. |
16010 |
File already exists. |
16011 |
Too many open files in the system. |
16012 |
Text file is busy. |
16013 |
File is too large. |
16014 |
File system is read only. |
16015 |
File locking deadlock. |
16016 |
Filename is too long. |
16017 |
|
16018 |
Bad or corrupted file system detected . |
TCP/IP ErrorIDs
ErrorID |
Description |
---|---|
16100 |
Connection error. |
16101 |
TCP ID has been closed. |
16102 |
All PLC TCP handles used. |
16103 |
TCP ID is invalid. |
16104 |
Failed to allocate TCP/IP socket. |
16105 |
TCP operation internal error. |